Hi,
I'm using the VEE 6.2 Automation Server to call some VEE functions with integrated Matlab code, and i have the next problem:
Each time I run my program i get a matlab.exe and a vee.exe alive processes in the Windows Task Manager.
If i run my program 10 times i get 20 processes (10 matlab and 10 vee processes eating Windows memory resources).
I use the Unload() method to close access to the vee library but it seems that vee.exe and matlab.exe are not really closed.
Is there any way to close vee.exe and matlab.exe after i use the VEE functions in the VEE Automation Server?
Thanks in advance for your help.
Regards.
Fran
-------------------------------------------------------------------------------------------------------------------
Este correo electrnico y, en su caso, cualquier fichero anexo al mismo, contiene informacin de carcter confidencial exclusivamente dirigida a su destinatario o destinatarios. Queda prohibida su divulgacin, copia o distribucin a terceros sin la previa autorizacin escrita de Indra. En el caso de haber recibido este correo electrnico por error, se ruega notificar inmediatamente esta circunstancia mediante reenvo a la direccin electrnica del remitente.
The information in this e-mail and in any attachments is confidential and solely for the attention and use of the named addressee(s). You are hereby notified that any dissemination, distribution or copy of this communication is prohibited without the prior written consent of Indra. If you have received this communication in error, please, notify the sender by reply e-mail
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
I've been extremely busy at work lately, to the point that I'd actually
stopped reading the VRF emails - I've got over 300 waiting to be perused!
However, I had to ask about something I've just noticed: Tho' I've got VEE
7, I've not used it much yet, 'cause I've not wanted to convert over the
existing tests right now (they're working fine, after all - if it ain't
broke, don't fix it, right?) However, I just opened a program which imports
a library of userfunctions that I've written previously, with VEE 7 (sorry,
written in VEE 6, opened with VEE 7), and it allowed me to edit an imported
function, even though it says view only at the top, as always. Is this a
new "feature" of VEE 7 , or a bug? The help says that you can't directly
edit an imported userfunction, just as before. Obviously, the edit can't be
saved, but I'm wondering why it's allowed in the first place?
Anybody else see this?
_____________________________________
Reiner Schlieker
Test Equipment Designer
Siemens Milltronics Process Instruments Inc.
Phone: (705) 740-7553
Fax: (705) 740-7692
Email: reiner.schlieker@siemens.com
Web: www.siemens-milltronics.com
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".