<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META http-equiv=Content-Type content="text/html; charset=windows-1255"><META content="MSHTML 5.50.4308.2900" name=GENERATOR><STYLE></STYLE></HEAD><BODY bgColor=#ffffff><DIV><FONT face=Arial size=2>hi all vrf</FONT></DIV><DIV><FONT face=Arial size=2></FONT> </DIV><DIV><FONT face=Arial size=2>please is there a sits which shows good example about some code in hpvee </FONT></DIV><DIV> </DIV><DIV><FONT face=Arial size=2>I will be very thankful to know</FONT></DIV><DIV> </DIV><DIV><FONT face=Arial size=2>regards</FONT></DIV><DIV><FONT face=Arial size=2>wisam</FONT> </DIV>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list, email "vrf@agilent.com". <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</BODY><br />-- <br />This message has been scanned for viruses and<br />dangerous content and is believed to be clean.</HTML>
>
I build application using hpvee5 .. this application work with acive x that
connected with excel .... this application was design on pc that was
installed on it windows 2000 and excel 2000...
I talk this application and install it into another pc which have windows 98
and excel 97 ... .... I see that I have some problem with moving that data
to excel .
is that case of different systems between the two PC
>
>
> Regards
> Wisam Alyan
> Phone-Or Ltd.
> Tel. 03-6344488 (Ext. 144)
> Fax 03-6349292
> Email: alyanw@Phone-or.com
>
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@it.lists.it.agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".