Hi Guys,
I have met one problem with unix controller systems, after boot testhead and type "testhead is 1", it comes out "system security problem detected".
It cause operator based mode can't be displayed on the system.
Please refer attached details of the problem
I'm appreciate if anyone can help.
Thanks
Regards,
David
I have met one problem with unix controller systems, after boot testhead and type "testhead is 1", it comes out "system security problem detected".
It cause operator based mode can't be displayed on the system.
Please refer attached details of the problem
I'm appreciate if anyone can help.
Thanks
Regards,
David
one thing to try from a unix shell window is to use the command boot 1, (that is boot ^space^ one)
and see what happens
thanks, Jon