AnsweredAssumed Answered

vrf NMEA 0183

Question asked by bwalden on Aug 16, 2004
I get a little disappointed ;-(  
Did not get any answer so far - unusual for the VRF...was the question so
strange ?

How do i set the SA 4411b in transmitting and receiving mode , so that it
works like a scalar network-analyzer,
and what it the fastest way to read out these datas then?

I need these infos because i do not have local access to this device to "try
and error" it ...


Any help wanted,
thanks in advance,
detlef


-----Ursprngliche Nachricht-----
Von: Baranski, Detlef [mailto:Detlef.Baranski@PILKINGTON.de]
Gesendet: 20 July 2004 12:20
An: VRF
Betreff: [vrf] FW: Spectrum analyser 4411b - S21 fast Trace readout ?


Thanks Paul.
I did find some info about it at the Agilent Web-Site.
So here is a conversion of the Spectrumanalyser-Program available at
www.my-vee.de for use with the 4411b SCIPI Commands.
Not all parts are adapted - see the comments.
Maybe it is of interest for someone.

But i still have the question:
How do i set the transmitter trace, and what is the fasted way to read out
this S21 ....is it still INT32 ?

I do not have local access to this SA anymore , therefore i am asking.

Enjoy the example!
best regards,
detlef



-----Ursprngliche Nachricht-----
Von: paul.2.rowan@bt.com [mailto:paul.2.rowan@bt.com]
Gesendet: 19 July 2004 15:55
An: VRF
Betreff: [vrf] FW: Spectrum analyser 4411b - S21 fast Trace readout ?


This is the piece of code I use to get traces. Never got around to finding
out why I needed the extra byte read ! Any suggestions, Andy?
I wish Agilent would provide this stuff with their analysers, it took a
couple of days of head scratching to get this working error free.
Regards
Paul Rowan
BT Goonhilly
This message and any attachments are confidential, for the exclusive use of
the addressee and may be legally privileged. Any other distribution, use or
reproduction is unauthorised and prohibited. If you have received this
message in error, please notify the sender immediately and delete the
message from your system.

Visit our internet site at http://www.pilkington.com
 


*** eSafe scanned this email for malicious content ***
*** IMPORTANT: Do not open attachments from unrecognized senders  ***
This message and any attachments are confidential, for the exclusive use of
the addressee and may be legally privileged. Any other distribution, use or
reproduction is unauthorised and prohibited. If you have received this
message in error, please notify the sender immediately and delete the
message from your system.

Visit our internet site at http://www.pilkington.com

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes