(VEE Pro 6.2)
>In initialization, set up a variable. Something like "cSTX = intToChar(2);"
Thanks for that.
While I'm on such a roll, is there a way to set the Direct I/O 'Read
Terminator' to ETX? My attempts at /003, ^C, etc, have come to naught.
TIA,
George
>In initialization, set up a variable. Something like "cSTX = intToChar(2);"
Thanks for that.
While I'm on such a roll, is there a way to set the Direct I/O 'Read
Terminator' to ETX? My attempts at /003, ^C, etc, have come to naught.
TIA,
George
Unfortunately, we are only using Vee 6 - So I can't do that.
B.R.
Martin
-----Original Message-----
From: ext pvergara@tqr.biz [mailto:pvergara@tqr.biz]
Sent: Tuesday, August 17, 2004 3:57 PM
To: Lentz Martin (Nokia-MP/Copenhagen)
Subject: Re: [vrf] E-mail sending from Vee
El Martes 17 Agosto 2004 15:33, martin.lentz@nokia.com escribi:
If you can use the .NET framework that have the VEE 7.0 Pro you can read the code example:
"Microsoft .Net Framework/SendMail.vee"
or use the object:
"System/SendMail"
> Hi VRF'ers
>
> In our test systems, we would like to add a feature, that it should be possible for the user to recieve an E-mail when the test has finished. As Outlook is not set up on the test system PCs, it is not a possibility to use that as an ActiveX, but does anybody have an example on how to use SMTP or WinSocket or something similar?
>
> B.R.
>
> Martin
>
>
> ---
> You are currently subscribed to vrf as: pvergara@tqr.biz
> To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
> To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
> To send messages to this mailing list, email "vrf@agilent.com".
> If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
>
--
----
Pablo C. Vergara Castro.
Departamento de informtica.
TQR-Software
Tlfno.: (+34) 986 11 46 40
Fax: (+34) 986 11 46 50
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".