Hi Again VRF,
I'm just writing back to say Er! Anyone ever notice that once you write
something down, the solution becomes obvious. Well, it happens to me!
So...Er...Duh...I figured out what I was doing wrong. Problem solved.
Thanks
Tom Daniels
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Hi VRF,
I have an issue with number conversion that is a real problem for me.
Hopefully it will be easy for one of you to explain to me.
I have a changing UInt8 array of approximately 300 bytes, that I need to
write out a serial port to a device in hexadecimal format. For a short
command, an IO write - Example (Write Binary 0x85, 0xFE, 0x55 BYTE) - works
great. To send the 300 bytes of UInt8 array data, though, I have trouble.
I can loop through and get each byte sent, but can't figure out how to get
the data converted and sent out in hex format from VEE.
Any help would be appreciated.
Best Regards,
Tom Daniels
Sr. Test Engineer
The Morey Corporation
100 Morey Drive
Woodridge, IL 60517
T: (630) 754-2256
F: (630) 754-2656
tdaniels@moreycorp.com
---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".