AnsweredAssumed Answered

vrf what's it?

Question asked by bill.ossmann on Nov 18, 2004
<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 3.2//EN"><HTML><HEAD><META HTTP-EQUIV="Content-Type" CONTENT="text/html; charset=us-ascii"><META NAME="Generator" CONTENT="MS Exchange Server version 5.5.2653.12"><TITLE>Mouse over panel</TITLE></HEAD><BODY><P><FONT SIZE=2 FACE="Arial">Hello all:</FONT></P><P><FONT SIZE=2 FACE="Arial">I am using a VEE program to acquire data from a VXI chassis and show it continuously in real time. I am using XY graphics to show data, and my problem is that even in runtime program, if I click the mouse onto the graphics it stop. The more dangerous part is that data acquisition is also stopped, so I can not, for example, do a graphic zoom. Is there any method to show data independent of other part of the program?. I am using VEE 6.0, is it a multithreading enviroment or not?</FONT></P><P><FONT SIZE=2 FACE="Arial">Regards</FONT></P><P><FONT COLOR="#000080" FACE="Comic Sans MS">Angel Cano</FONT><BR><FONT COLOR="#000080" FACE="Comic Sans MS">Test Department</FONT><BR><FONT COLOR="#000080" FACE="Comic Sans MS">email: angel.cano@itp.es</FONT></P>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list,  email "vrf@agilent.com".  <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</BODY></HTML>  

Outcomes