AnsweredAssumed Answered

vrf E5810 lan2gpib converter and VEE 6.2 basic problem

Question asked by rsb on Nov 30, 2004
Fred Enz <Fred.Enz@enz-berlin.de> wrote:
> Has anybody used E5810  lan2gpib converter with VEE 6.2 ?
> I set the 5810 parameter to
> - GPIB SICL Interface Name :  gpib14
> - GPIB Address:  21
> - GPIB Logical unit:  7

> If I add GPIB10 manually and create a new instrument as 1015 and try to
> send a string,
> the error 801:
> Configuration error: GPIB interface, at 10, is not configured for this
> system.
>
> What is wrong??

Your above note says that the interface name is GPIB14 and the
logical unit is _7_  so you need to add gpib14 and then look at address 715

Stan


--------------------------------------------------------------------------
Stan Bischof  Agilent Technologies  707-577-3994  stan_bischof@agilent.com
--------------------------------------------------------------------------

---
You are currently subscribed to vrf as: rsb@soco.agilent.com
To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".

Outcomes