AnsweredAssumed Answered

Direct I/O problem

Question asked by VRFuser on Nov 27, 1996
Hans van der Zanden wrote:
>
> HP Vee users,
>
> I'm using HPVee Version 3.21. with te following instruments:
>
> * HP multimeter 3458A
> * HP mainframe E1301
> * thermocouplecard 1345
> * "              " 1347
> * ext...
>
> I've got no problem with the direct I/O and the external multimeter,
> but when i send a command to the thermocouplecard (1345 or 1347),
> nothing happends. When i take a instrument panel from this card,
> everything works oke.
>
> I also see no data comming from the thermocouplecard when i use the I/O
> bus monitor.
>
> I would grateful if anyone could help me to solve this problem.
>
> Thanks
>
> Hans van der Zanden
> AWB BV Beek en Donk
> The Netherlands
> Email: j.van.der.zanden@tip.nl

Outcomes