AnsweredAssumed Answered

VRf_Vee problems Seriuos error + at little problem

Question asked by VRFuser on Jul 22, 1996

>> Is this a repeatable problem?  Or did it just happen once?

>I've run into this several times. I have a UserObject with panel view.
>In detail view I 'cut' something (one time, I think it was label) which
>has
>been visible in panel view. Then I change to panel view. The label is
>still
>visible there, and when I put the mouse cursor on it I get these
>horrifying bright-red messages about internal errors, messages to
>non-existent objects, possibly corrupted program, and contacting HP
>support.

>Sorry about not being more precise, haven't had time to chase the bug.
>Don't know the exact steps to repeat it; of course it does not happen
>every time in the abovenetioned scenario. As a preventive medicine, I
>try to
>remember to delete objects first in panel view, then cut them in detail
>view.

>Oh yes the system: HP VEE 3.2 and Win95. Various 486s and Pentiums
>with 16 MB of RAM. Self-written serial communications with educational
>measurement gear.


My eqip. : Pentium 133Mhz 32 MB ram Win NT Vee 3.20

it must be a bug !

------------ new problem -------------
Another thing : I save some data on a unix, and transfer via Ftp to a PC
and  try to read the file into Excell it looks like this :

Data;data
Empty line
Data;Data
Empty line
etc.

The line is about 660 chars and is terminated by a 0DH 0AH. That is CR
LF, so i cant understand why it fails.

The line consist og Date & time+120 Meas. Values+120 Limits values

properly something about EOL char. Anyone got the solution ?


  _________
  /    |   
   0   |What a beautiful day,
-||-  |my regards to the man
  /   |who invented sunglases

  Henrik Grevelund
mkpkor@inet.uni-c.dk

Ill bee back !

Outcomes