for VRf HP VEE help
I have a list of tests that will be changing so I want to avoid hard-coding
their names.
The tests are stored in a library and the test names are also stored in a
dataset.
I would like to run these tests in a sequencer, but it will not let you pass
in the function
name. So, instead, I send the names one by one into a "call function"
object and then
feed the output into a sequencer. The problem I have now is that I can only
have one
test in the sequencer log record. I can not do a "merge record" because the
field names
are the same.
So my questions are:
1. Is there a way of sending the function name into a sequencer?
2. Is there a way of changing a field name in a record?
BTY... I am running VEE 3.12 under Windows 3.1 and HP_UX 9
Thanks for any help
p27676@email.mot.com