Hi all!
I have the following problem:
I use the Recorder in Windows 3.11 to control an emulator for the
Motorola MC68360 CPU. The emulator program cant be
controlled from any other program.
With two macros saved in the same macro-file, I can control the
emulator simulating keyboard commands.
Theese macros I can run from HP-VEE 3.12 with the Execute program
object.
The commands looks like:
Recorder.exe -h F1 trbdm.rec (F1 is the shortcutkey to start macro1)
and
Recorder.exe -h F2 trbdm.rec (F2 is the shortcutkey to start macro2)
Theese commands works if the recorder is closed after running each
command, but the recorder doesn't close, and I have to do it
manually.
Is there a way to close applications in Windows 3.11 from HP-VEE,
maybe using the taskmanager application with command line options?
Thanks
Bjorn Kristian Kleven
______________________________
Bjoern Kristian Kleven
Ericsson AS
Norway
______________________________
Mail: etobkle@eto.ericsson.se
Memo: ETO.ETOBKLE
Fax: +47 66 98 10 95
Phone: +47 66 84 16 03
______________________________
I have the following problem:
I use the Recorder in Windows 3.11 to control an emulator for the
Motorola MC68360 CPU. The emulator program cant be
controlled from any other program.
With two macros saved in the same macro-file, I can control the
emulator simulating keyboard commands.
Theese macros I can run from HP-VEE 3.12 with the Execute program
object.
The commands looks like:
Recorder.exe -h F1 trbdm.rec (F1 is the shortcutkey to start macro1)
and
Recorder.exe -h F2 trbdm.rec (F2 is the shortcutkey to start macro2)
Theese commands works if the recorder is closed after running each
command, but the recorder doesn't close, and I have to do it
manually.
Is there a way to close applications in Windows 3.11 from HP-VEE,
maybe using the taskmanager application with command line options?
Thanks
Bjorn Kristian Kleven
______________________________
Bjoern Kristian Kleven
Ericsson AS
Norway
______________________________
Mail: etobkle@eto.ericsson.se
Memo: ETO.ETOBKLE
Fax: +47 66 98 10 95
Phone: +47 66 84 16 03
______________________________