AnsweredAssumed Answered

VRF-Scrollbar_Problem

Question asked by VRFuser on Aug 15, 1996
send q VRF-Scrollbar_Problem vrf

from: Greg Goebel / HP-MXD
      gvg@lvld.hp.com / 970-679-2305 / FAX 970-679-5971
to:   HG / VRf
date: Friday, 16 August 1996 1442 MDT

> I am witness to a strange behaviour :
>
> The scrollbars in Detail view dosn't get updated when a popup-object has
> been covering them.
>
> In Panel view that isn't any problem because there is no scrollbar.
>
> My machine :
> V743 with 64 MB Ram
> HP UX A.09.05
> HP VEE 3.20  Feb. 22, 1996

Sir:

I am having troubles figuring out what the problem is here.  I tried to
put a NotePad on the display and added text until it had scrollbars ... I
generated a Message Box popup over the top of it and when it went away, the
NotePad was unchanged.

Then I wrote a little program to force a Logging Alphanumeric to scroll
continuously, updated with the time, along with a second parallel program to
generate a popup.  In this configuration, the popup simply would flash up
and then vanish while the AlphaNumeric spun on its merry little way.

So I merged the two programs as separate branches.  When I generated the
popup, it stopped the AlphaNumeric (to be expected); when I got rid of it,
the AlphaNumeric started clocking time where it left off.

Now I don't see how I could get the popup to fall on the scrollbars at the
edge of the VEE border in any reasonable way, since it normally comes up
more or less centered.

So, enlighten me, please ... do you have a little example with some notes
that can give me a path to the problem.

[<>] regards -- gvg

Outcomes