AnsweredAssumed Answered

Vrf- Annoing behaviour in Text Constant

Question asked by VRFuser on Aug 21, 1996
>From :  Henrik Grevelund
     mkpkor@inet.uni-c.dk


Greetings

I have some problems with a Text Constant object. I use it to show
remarks, to explane some other datafile.

The array of remarks are not always the same, and when i send it to the
text Constant the size will go back to default, but only if the previus
remarks are another arraysize. And that is very Annoing.

When you put the text Constant on the panel it would be nice if it would
keep the same size !

I have made an example, if anyone want it then toss a mail to me.

|repeat|
        |
   -----|
   |    |
   |  |OK|---|text constant 1| 
   |    |    |0000:1         |
   |  |next| |0001:2         |----
   |         |0002:3         |    |
   |          |0003:4         |    |
   |----|                         |---|   |  |Text constant 3   |
        |                             |JCT|  |0000:             |
      |OK|---|text constant 2|        |   |--|0001:             |
       |    |0000:1         |    |---|   |  |0002:             |
      |next| |0001:2         |    |
             |0002:3         |    |          input is default value
          |0003:4         |----
             |0004:5         |
          |0005:6         |
             |0006:7         |

Make Text constan 3 big, and start the program and press one OK, and Text
Constant will change size BUMMER !



What a HAPPY day, The sun is shining, and the girls are almost naked
on the beach.
____________________
/  Henrik Grevelund 
|mkpkor@inet.uni-c.dk|
----------------------
  /              /
/              / 

Outcomes