I am using the analog meter for doing an adjustment. In my test program,
where I hand entered the values in the properties it worked fine. I was
using just the red and green colors. Now I am trying to create a generic
function that allows the min and max values to be set. When I add the
terminals for the min and max all I get is the green range.
Can the green min and max be set as well as the red min and max,
programatically? If so how does one do it?
I am doing this in HPVee 3.12.
Thanks for the help.
Mike Gustin
mgustin@smsmfg.sms.siemens.com