AnsweredAssumed Answered

VRF-Meter_Object

Question asked by VRFuser on May 6, 1997
send q VRF-Meter_Object ww vrf mgustin@smsmfg.sms.siemens.com

from: Greg Goebel / HP-MXD
      gvg@lvld.hp.com / 970-679-3030 / FAX 970-679-5971
to:   Mike Gustin
date: Tuesday, 06 May 1997 1554 MDT

> I am using the analog meter for doing an adjustment. In my test program,
> where I hand entered the values in the properties it worked fine. I was
> using just the red and green colors. Now I am trying to create a generic
> function  that allows the min and max values to be set.  When I add the
> terminals for the min and max all I get is the green range.
>
> Can the green min and max be set as well as the red min and max,
> programatically? If so how does one do it?

Sir:

No can do in 3.12 ... we did add these features in VEE 4.0, however.

> I am doing this in HPVee 3.12.
>
> Thanks for the help.
> Mike Gustin
> mgustin@smsmfg.sms.siemens.com

If you have more questions, let us know.

[<>] regards -- gvg

Outcomes