AnsweredAssumed Answered

Re2: VRf VEE remote access w/NI card

Question asked by VRFuser on Jul 22, 1997
"Tom Sanders" <toms@symca.com> wrote:
>
> If you are using VEE or any other language that uses SICL this should be
> straightforward.  On PC2 configure as a LAN client (depending on version this
> is done under SICL config or HP I/O libraries-IO config).  On PC1 configure as
> a LAN server, then start the service manager (depending on version this is
> called siclland.exe or sm.exe). 

Should be, sure.

However this came up locally a few months back and it was explained
to me that SICL and NI were incompatible in this respect. That is you
could set up an HP card but not the NI.

HOWEVER- I'd sure like to hear if anyone gets this working, especially
for the NI PCMCIA GPIB.

Stan Bischof
stanb@sr.hp.com


Outcomes