--- On Wed, 28 May 1997 08:49:59 -0700 Mike Groves <mike.groves@ericsson.com> wrote:
> To: Vee Reflector
> From: mike.groves@ericsson.com
> Subject: Follow-up: Focus broke?
> Platform: VEE 4.0, HP Vectra Pentium, WinNT 4.0
>
>
> I made an error in my definition of the focus problem.
> If you connect a START button to the sequence pins of
> the OK buttons that are to be shown on the pop-up panel,
> it seems to work as defined. If you change the START
> to a REPEAT UNTIL BREAK, then the problem exists where
> the upper left OK is not always the one in focus. If
> it is, break the sequence wire to it and re-connect it.
> The focus will now change to another OK button ignoring
> positioning on the panel. Save it and recall it and
> the position sometimes changes again.
>
> -Mike
>
>
---------------End of Original Message-----------------
Mike,
If you use a REPEAT UNTIL BREAK to hit an OK button, you need a seperate one for each OK button.
--------------------------------------------------------
Name: Tom Sanders, Symtx (formerly Symmetrix)
Date: 05/29/97 Time: 17:00:59
--------------------------------------------------------