AnsweredAssumed Answered

vrf-dll vee 4.01

Question asked by VRFuser on Jul 14, 1997
Sandra Koppen wrote:
>
> VRf
>
> ************
> I wrote and successfully executed a DLL using Borland 5.0 and VEE 3.2, but
> when I ported it to another computer running VEE 4.01 I get the error
> message when trying to import the library - "cannot execute <filename>". I
> have VEE 3.2 running on a pentium PC and VEE 4.01 on another pentium PC
> both using Windows 95.  Am I missing a compiler switch or what do you think
> the problem might be???  Any direction is helpful.
> ************
> Thanks for the fast responses. Here is more information.
> I used Borland to compile the DLL as 32 bit using DllEntryPoint().  When I
> import the library from within VEE I set the path for the DLL and the *.h
> in the inport library object. Any more ideas are appreciated.
>
> Thanks,
> Sandra Koppen
> NASA LaRC
> Hampton, VA
> s.v.koppen@larc.nasa.gov

Sandra

First are you shure your importing the library and not trying to execute
it in vee 4 the import box if i remember right also execute. you need to
select the appropriate action desired.I think i am a home now not in the
lab so i cant check, but i wll verify it tomorrow!
hope this help?
But using BC is using the hard road!!
I do not prefer MS but they built the OS and their product are
compatible in the long run!!!

Marc Y. Lord
Bell Helicopter Textron Canada
System Integration Lab.

Outcomes