From: Tim Axness
To: VRF
I implemented an ABORT TEST using the technique Greg Goebel suggested. Just
place an OK button with an Exit UserObject on a parallel thread to the test
sequence. The ABORT is executed almost immediately after being activated. I
found this works well, but you have to structure your vee code well to get
determinate flow.
> I would also like to see some of the things Juan has suggested here, they
> would be very usefull. For example, when we are executing a series of
> tests
> we want the operator to have the ability to ABORT the test sequence at
> any given time. We had to implement this just as Greg had suggested using
> a showpanel() with a self resetting toggle which we poll in between each
> test.
>
> In order to have just one, much less two, input box operate (I call it
> asynchronous input for
> want of a better term) as suggested, it would have to be input by another
> process
> (a process running outside of VEE) and would have to interrupt VEE. This
> could
> be built into VEE in a future release if enough VEE users really need it.
> It would
> work something like this:
>
> When an input function is called in VEE, VEE spawns another process
> with it's own window to input the data and provides an interrupt service
> routine to handle the interrupt from the spawned input process when
> it completes (via input, cancel, timeout or whatever).
>
> The reason for an external process has to do with multi-threading,
> which Juan pointed out that one instance of a function blocks
> another until the first is completed. This is inherent in
> multi-threading.
> To have two or more at the same time requires two or more instances
> of the same block of code residing in memory at the same time, which
> is known as multi-tasking and requires miltiple processes to accomplish.
>
> Even using re-entrant code would not solve this because only one
> entry could execute at any given time.
>
> Another option would be to have VEE generate in-line code for these
> functions which could then be executed separately - the only trick
> would be to keep track of which one gets the inputs from the keyboard
> and/or other devices at any given time (when using a separate process,
> the window manager
> takes care of that for you).
>
> These would be nice features and probably not too hard to implement.
> VEE has been on a very impressive upgrade path which has made great
> improvements so far, maybe we can get this in VEE 5.0 ???
>
> Regards
>
> Rob Marquardt
> System Test Engineering
> Rockwell Automation / Allen-Bradley
> Milwaukee, Wisconsin, USA
>
>
>
>
>
> ********** Juan's comments **********
>
> However I have several comments to the hidepanel solution.
> The problem, from my point of view, is that there are some objects (with
> input or output information) that stop the application until an input
> from
> the user is performed. Therefore (an for example), if a message box is
> used,
> while the message is displayed on the screen, the rest of the application
> is
> stopped.
>
> * This panel solution has not the same performances than a Dialog Box
> Integer Input, for example. This object implements a timeout and checks
> if
> the input is included in some limits. Therefore, if we need these
> features,
> we should include them in the function of the panel increasing its
> complexity and our work.
>
> * There are several objects with the mentioned characteristics which
> allow
> you to perform a interface with the user of the application: all objects
> Dialog Box objects (Text Input, Real Input, Integer Input, List Box,
> Message
> Box and File Name Selection). Therefore, if we need to have the same of
> one
> of them, we should develop the corresponding function to perform "the
> same
> functionality" but being able of not stopping the application. But the
> original VEE objects has been tested and they are developed at a lower
> level, therefore their performances should be better that the equivalent
> user developed functions with hide panels.
>
> * On the other hand, it should be taken into account that for VEE V3.X,
> when
> a user function is activated, the application does not work with other
> thread until all the function has been wholly executed. Then we get the
> same
> problem: until the user writes one input the execution flow of the rest
> of
> the application is stopped. Although this does not happen in V4.0,
> because
> in this version a function and other external (to the mentioned function)
> object can be executed at the same time. However we cannot execute the
> same
> function (with different parameters) at the same time. That means that
> VEE
> does not allow to provide two different operator messages at the same
> time
> (using the same Message Box object or the same equivalent user developed
> function).
>
> I think of showing on the screen different messages (of different
> equipment,
> for example) at the same time (each of them has a timeout in order to be
> vanished if the operator is not on line) in a monitoring project is very
> common. But the monitoring of the equipment cannot be stopped until these
> messages has been removed from the screen. This should be compatible with
> an
> application that does not have a collection with a lot of different and
> user
> developed functions (which are very expensive to develop and maintain) to
> show operator messages (alarms, warnings, information, executed commands,
> etc.). And more, taken into account that VEE provides some similar
> objects.
>
> In order to avoid that, I suggested that all interface object could have
> a
> switch in such a way that when it is raised the object acts like a wait
> (of
> the timeout if it is included) until the operator push a OK (for the
> message) or write an input. Meanwhile the rest of the application
> continues
> executing.
>
>
--
*****************************
Timothy A. Axness
taa@orion.jhuapl.edu
Applied Physics Laboratory
Johns Hopkins University
*****************************
To: VRF
I implemented an ABORT TEST using the technique Greg Goebel suggested. Just
place an OK button with an Exit UserObject on a parallel thread to the test
sequence. The ABORT is executed almost immediately after being activated. I
found this works well, but you have to structure your vee code well to get
determinate flow.
> I would also like to see some of the things Juan has suggested here, they
> would be very usefull. For example, when we are executing a series of
> tests
> we want the operator to have the ability to ABORT the test sequence at
> any given time. We had to implement this just as Greg had suggested using
> a showpanel() with a self resetting toggle which we poll in between each
> test.
>
> In order to have just one, much less two, input box operate (I call it
> asynchronous input for
> want of a better term) as suggested, it would have to be input by another
> process
> (a process running outside of VEE) and would have to interrupt VEE. This
> could
> be built into VEE in a future release if enough VEE users really need it.
> It would
> work something like this:
>
> When an input function is called in VEE, VEE spawns another process
> with it's own window to input the data and provides an interrupt service
> routine to handle the interrupt from the spawned input process when
> it completes (via input, cancel, timeout or whatever).
>
> The reason for an external process has to do with multi-threading,
> which Juan pointed out that one instance of a function blocks
> another until the first is completed. This is inherent in
> multi-threading.
> To have two or more at the same time requires two or more instances
> of the same block of code residing in memory at the same time, which
> is known as multi-tasking and requires miltiple processes to accomplish.
>
> Even using re-entrant code would not solve this because only one
> entry could execute at any given time.
>
> Another option would be to have VEE generate in-line code for these
> functions which could then be executed separately - the only trick
> would be to keep track of which one gets the inputs from the keyboard
> and/or other devices at any given time (when using a separate process,
> the window manager
> takes care of that for you).
>
> These would be nice features and probably not too hard to implement.
> VEE has been on a very impressive upgrade path which has made great
> improvements so far, maybe we can get this in VEE 5.0 ???
>
> Regards
>
> Rob Marquardt
> System Test Engineering
> Rockwell Automation / Allen-Bradley
> Milwaukee, Wisconsin, USA
>
>
>
>
>
> ********** Juan's comments **********
>
> However I have several comments to the hidepanel solution.
> The problem, from my point of view, is that there are some objects (with
> input or output information) that stop the application until an input
> from
> the user is performed. Therefore (an for example), if a message box is
> used,
> while the message is displayed on the screen, the rest of the application
> is
> stopped.
>
> * This panel solution has not the same performances than a Dialog Box
> Integer Input, for example. This object implements a timeout and checks
> if
> the input is included in some limits. Therefore, if we need these
> features,
> we should include them in the function of the panel increasing its
> complexity and our work.
>
> * There are several objects with the mentioned characteristics which
> allow
> you to perform a interface with the user of the application: all objects
> Dialog Box objects (Text Input, Real Input, Integer Input, List Box,
> Message
> Box and File Name Selection). Therefore, if we need to have the same of
> one
> of them, we should develop the corresponding function to perform "the
> same
> functionality" but being able of not stopping the application. But the
> original VEE objects has been tested and they are developed at a lower
> level, therefore their performances should be better that the equivalent
> user developed functions with hide panels.
>
> * On the other hand, it should be taken into account that for VEE V3.X,
> when
> a user function is activated, the application does not work with other
> thread until all the function has been wholly executed. Then we get the
> same
> problem: until the user writes one input the execution flow of the rest
> of
> the application is stopped. Although this does not happen in V4.0,
> because
> in this version a function and other external (to the mentioned function)
> object can be executed at the same time. However we cannot execute the
> same
> function (with different parameters) at the same time. That means that
> VEE
> does not allow to provide two different operator messages at the same
> time
> (using the same Message Box object or the same equivalent user developed
> function).
>
> I think of showing on the screen different messages (of different
> equipment,
> for example) at the same time (each of them has a timeout in order to be
> vanished if the operator is not on line) in a monitoring project is very
> common. But the monitoring of the equipment cannot be stopped until these
> messages has been removed from the screen. This should be compatible with
> an
> application that does not have a collection with a lot of different and
> user
> developed functions (which are very expensive to develop and maintain) to
> show operator messages (alarms, warnings, information, executed commands,
> etc.). And more, taken into account that VEE provides some similar
> objects.
>
> In order to avoid that, I suggested that all interface object could have
> a
> switch in such a way that when it is raised the object acts like a wait
> (of
> the timeout if it is included) until the operator push a OK (for the
> message) or write an input. Meanwhile the rest of the application
> continues
> executing.
>
>
--
*****************************
Timothy A. Axness
taa@orion.jhuapl.edu
Applied Physics Laboratory
Johns Hopkins University
*****************************