Stan Bischof wrote:
>
> "Gustin, Mike" <mgustin@smsmfg.sms.siemens.com> wrote:
> >
> > I would appreciate help with this problem.
> >
> > I am currently using 3.12 running on windows 3.11. My processor is an intel
> > 133MHz Pentium.
> >
> > I am using a "To File" object in my program twice in both cases it is
> > writting to the same file. The first instance is in my main program where I
> > write header information to the file. This instance has the box for clearing
> > the file at prerun checked. The second instance is in an imported vee
> > routine.
> > The box is not checked to clear the file at prerun in that test program.
> >
> > When the main program is run and the second instance "To File" is imported
> > the check box for clearing the file is checked off. The orginal program does
> > not have it checked but the imported version is checked to clear.
> >
> > How do you fix this problem???
>
> Remember that the file system allows exactly _one_ write pointer to
> a given file from your VEE process. This is not a VEE issue per se
> but rather is a basic function of the OS and file system.
>
> What this means inside VEE is that all the TO FILE objects referring to
> a given file must share the same pointer. Hence they also must
> share attributes such as "clear the file at prerun".
>
> Now, in your case, just what is the "problem" that needs to get fixed?
>
> It sounds like you want your file to be cleared at prerun. And I'm guessing
> that your imported routine wants to append to the file rather than
> clearing it? If so you shouldn't have any problems.
>
> Another way of looking at this:
>
> Your VEE program is writing to exactly one file. You have
> multiple TO FILE objects. It would make no sense for one of them
> to say "clear the file at prerun" and another to say
> "don't clear the file at prerun". Can't have it both ways, given that
> prerun occurs exactly once!
>
> Perhaps I'm missing the point. Please explain further what you are trying
> to do and what isn't working.
>
> regards
>
> Stan Bischof
> stanb@sr.hp.com
The above explenation of Stan is clear. Others pointed out to use a To/File object
with a clear action and DON'T have the 'Clear File at pre-run' boxes checked.
Some remarks from my side:
1. Same problems hold for To/From dataset. There is, however no, no
'transaction-block'. You always need seperate T0File objects.
2. Why is the 'Clear File at pre-run' box still active when you have a control
pin for the filename attached to the object? Using a Filename input clearly
indicates that the filename and so the filepointer too are to be determined
during programm execution. Perhaps it should also be an regular input
i.s.o. a control input.
3. Why are there differences in the nummer of available control-inputs between
To/From file and To/From dataset objects. In my oppinion they are basically
the same; ToFrom dataset has additional features for schema/data, reflected
in somewhat different behaviour of 'Rewind' and 'Clear'. Why same names than?
I once saved a lot of data through a To Dataset objects in a UserFunction with
the name MyFile on it, but with a FileName control input. When I wanted to do
similar measurements some weeks later, I had to build a simple test first.
This test also used a ToFile object but with 'Clear File at pre-run' box checked.
(So also the box in the libarie became checked!!!!) When finally starting the
measurements, I could not append any data to files anymore: the old data was
overwritten!!!
I recommend HP to change vee so that behaviour as from above can not occure anymore.
At least you can put warning signs on the object, manuals, etc....
Remi.
------------------------------------------------
Remi Tuijtelaars,
Philips Semiconductors, Dev. T&D, BZ-2.090
Gerstweg 2, 6534 AE Nijmegen, The Netherlands
tel: +31-24-353-2812 fax: +31-24-353-3160
mailto: Remi.Tuijtelaars@nym.sc.philips.com
------------------------------------------------
>
> "Gustin, Mike" <mgustin@smsmfg.sms.siemens.com> wrote:
> >
> > I would appreciate help with this problem.
> >
> > I am currently using 3.12 running on windows 3.11. My processor is an intel
> > 133MHz Pentium.
> >
> > I am using a "To File" object in my program twice in both cases it is
> > writting to the same file. The first instance is in my main program where I
> > write header information to the file. This instance has the box for clearing
> > the file at prerun checked. The second instance is in an imported vee
> > routine.
> > The box is not checked to clear the file at prerun in that test program.
> >
> > When the main program is run and the second instance "To File" is imported
> > the check box for clearing the file is checked off. The orginal program does
> > not have it checked but the imported version is checked to clear.
> >
> > How do you fix this problem???
>
> Remember that the file system allows exactly _one_ write pointer to
> a given file from your VEE process. This is not a VEE issue per se
> but rather is a basic function of the OS and file system.
>
> What this means inside VEE is that all the TO FILE objects referring to
> a given file must share the same pointer. Hence they also must
> share attributes such as "clear the file at prerun".
>
> Now, in your case, just what is the "problem" that needs to get fixed?
>
> It sounds like you want your file to be cleared at prerun. And I'm guessing
> that your imported routine wants to append to the file rather than
> clearing it? If so you shouldn't have any problems.
>
> Another way of looking at this:
>
> Your VEE program is writing to exactly one file. You have
> multiple TO FILE objects. It would make no sense for one of them
> to say "clear the file at prerun" and another to say
> "don't clear the file at prerun". Can't have it both ways, given that
> prerun occurs exactly once!
>
> Perhaps I'm missing the point. Please explain further what you are trying
> to do and what isn't working.
>
> regards
>
> Stan Bischof
> stanb@sr.hp.com
The above explenation of Stan is clear. Others pointed out to use a To/File object
with a clear action and DON'T have the 'Clear File at pre-run' boxes checked.
Some remarks from my side:
1. Same problems hold for To/From dataset. There is, however no, no
'transaction-block'. You always need seperate T0File objects.
2. Why is the 'Clear File at pre-run' box still active when you have a control
pin for the filename attached to the object? Using a Filename input clearly
indicates that the filename and so the filepointer too are to be determined
during programm execution. Perhaps it should also be an regular input
i.s.o. a control input.
3. Why are there differences in the nummer of available control-inputs between
To/From file and To/From dataset objects. In my oppinion they are basically
the same; ToFrom dataset has additional features for schema/data, reflected
in somewhat different behaviour of 'Rewind' and 'Clear'. Why same names than?
I once saved a lot of data through a To Dataset objects in a UserFunction with
the name MyFile on it, but with a FileName control input. When I wanted to do
similar measurements some weeks later, I had to build a simple test first.
This test also used a ToFile object but with 'Clear File at pre-run' box checked.
(So also the box in the libarie became checked!!!!) When finally starting the
measurements, I could not append any data to files anymore: the old data was
overwritten!!!
I recommend HP to change vee so that behaviour as from above can not occure anymore.
At least you can put warning signs on the object, manuals, etc....
Remi.
------------------------------------------------
Remi Tuijtelaars,
Philips Semiconductors, Dev. T&D, BZ-2.090
Gerstweg 2, 6534 AE Nijmegen, The Netherlands
tel: +31-24-353-2812 fax: +31-24-353-3160
mailto: Remi.Tuijtelaars@nym.sc.philips.com
------------------------------------------------