<!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.0 Transitional//EN"><HTML><HEAD><META HTTP-EQUIV="Content-Type" CONTENT="text/html; charset=iso-8859-1"><TITLE>Mouse over panel</TITLE><META content="MSHTML 6.00.2800.1476" name=GENERATOR></HEAD><BODY><DIV><SPAN class=265231609-19112004><FONT face=Arial color=#0000ff size=2>Angel, you have a problem.</FONT></SPAN></DIV><DIV><SPAN class=265231609-19112004><FONT face=Arial color=#0000ff size=2>Vee is not multithreading.</FONT></SPAN></DIV><DIV><SPAN class=265231609-19112004><FONT face=Arial color=#0000ff size=2>To reduce the effect of the mouse over, just use the "short click " and go further function of a button. But there will be always a short delay.</FONT></SPAN></DIV><DIV><SPAN class=265231609-19112004><FONT face=Arial color=#0000ff size=2>MAybe someone else have a better description or a solution for this.</FONT></SPAN></DIV><DIV><SPAN class=265231609-19112004><FONT face=Arial color=#0000ff size=2>Maybe you have to use 2 Vee programs, one for data aquisition and one for further User Interface functionality...</FONT></SPAN></DIV><DIV><SPAN class=265231609-19112004><FONT face=Arial color=#0000ff size=2></FONT></SPAN> </DIV><DIV><SPAN class=265231609-19112004><FONT face=Arial color=#0000ff size=2>best regards,</FONT></SPAN></DIV><DIV><SPAN class=265231609-19112004><FONT face=Arial color=#0000ff size=2>detlef</FONT></SPAN></DIV><DIV><SPAN class=265231609-19112004></SPAN> </DIV><BLOCKQUOTE> <DIV class=OutlookMessageHeader dir=ltr align=left><FONT face=Tahoma size=2>-----Ursprngliche Nachricht-----<BR><B>Von:</B> Cano Soler, Angel [mailto:angel.cano@itp.es]<BR><B>Gesendet:</B> Freitag, 19. November 2004 09:04<BR><B>An:</B> VRF<BR><B>Betreff:</B> [vrf] Mouse over panel<BR><BR></FONT></DIV> <P><FONT face=Arial size=2>Hello all:</FONT> </P> <P><FONT face=Arial size=2>I am using a VEE program to acquire data from a VXI chassis and show it continuously in real time. I am using XY graphics to show data, and my problem is that even in runtime program, if I click the mouse onto the graphics it stop. The more dangerous part is that data acquisition is also stopped, so I can not, for example, do a graphic zoom. Is there any method to show data independent of other part of the program?. I am using VEE 6.0, is it a multithreading enviroment or not?</FONT></P> <P><FONT face=Arial size=2>Regards</FONT> </P> <P><FONT face="Comic Sans MS" color=#000080>Angel Cano</FONT> <BR><FONT face="Comic Sans MS" color=#000080>Test Department</FONT> <BR><FONT face="Comic Sans MS" color=#000080>email: angel.cano@itp.es</FONT> </P>---<BR>You are currently subscribed to vrf as: Detlef.Baranski@PILKINGTON.de<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list, email "vrf@agilent.com". <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com". </BLOCKQUOTE>---<BR>You are currently subscribed to vrf as: rsb@soco.agilent.com<BR>To subscribe send a blank email to "join-vrf@it.lists.it.agilent.com".<BR>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".<BR>To send messages to this mailing list, email "vrf@agilent.com". <BR>If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".</BODY></HTML><P><FONT SIZE=2 FACE="Arial">This message and any attachments are confidential, for the exclusive use of the addressee and may be legally privileged. Any other distribution, use or reproduction is unauthorised and prohibited. If you have received this message in error, please notify the sender immediately and delete the message from your system. </FONT></P><BR><P><FONT SIZE=2 FACE="Arial">Visit our internet site at http://www.pilkington.com</FONT></P>