AnsweredAssumed Answered

IO Config problems in Runtime

Question asked by VRFuser on Jan 24, 1998
When I attempt to run ioconfig for serial ports or GPIB card, I get an
error message that there is already a device present.  If I delete the
devices and reconfigure them again I have to go to the next higher address
or I get the same message again. Each time I try this the address bumps up
one.  Even when the devices appear to configure successfully I get an error
that the config is not correct for this system. This is VEE 4.0 runtime on
a Win '95 machine.

Dave Rust  (drust@doitnow.com)
Test Engineer
Celwave RF
Phoenix, AZ


Outcomes