Hi,
I finally got HP VEE v4.0. In going through some of the examples, I
noticed that I couldnt move around in a panel the way I can in the Main
Window. There isnt even any scroll bars available in this MDI window.
If there is a way, its not readily available in the help. At the
moment, my only solution is to increase the resolution to 1024x1024 or
greater. Is there another way????
Thanks,
I finally got HP VEE v4.0. In going through some of the examples, I
noticed that I couldnt move around in a panel the way I can in the Main
Window. There isnt even any scroll bars available in this MDI window.
If there is a way, its not readily available in the help. At the
moment, my only solution is to increase the resolution to 1024x1024 or
greater. Is there another way????
Thanks,
gvg@lvld.hp.com / 970-679-3030 / FAX 970-679-5971
to: Vrf -- Ron Desgrosiers
date: Thursday, 19 June 1997 1030 MDT
Hi ... please add "VRf" to the title of your messages. Also, a nice little
header might be useful to ensure that people understand who to get in touch
with, or have a phone number in case your email breaks. (Email is NOT very
reliable.)
> I finally got HP VEE v4.0. In going through some of the examples, I
> noticed that I couldn=92t move around in a panel the way I can in the Mai=
> n
> Window. There isn=92t even any scroll bars available in this MDI window.=
Huh? I have them here. I suspect your window might be loading bigger than
the display and you can't see them. Try using the Window->Tile entries to
get a Window that fits in the screen.
If that doesn't help, an example might let me understand what is happening.
> If there is a way, it=92s not readily available in the help. At the
> moment, my only solution is to increase the resolution to 1024x1024 or
> greater. Is there another way????
>
> Thanks,
Please stay in touch.
[<>] regards -- gvg