Hi, Drew
I use an array of records and the variable that contains information of a
number of using records, which are declared as global. I know only one
inconvenience that it is impossible to write an array which size is different
from the declared.
With best regards,
Mikhail Kozlov kozlov@vniief.ru
I use an array of records and the variable that contains information of a
number of using records, which are declared as global. I know only one
inconvenience that it is impossible to write an array which size is different
from the declared.
With best regards,
Mikhail Kozlov kozlov@vniief.ru
I'm working with a process that collects data from a list of devices that
varies in size from one run to the next. Sometimes there is only a reference
and one test device up to N test devices. My limit right now is 3 but it could
be N.
My problem is passing information for the devices from one block to the next
and deciding in each block how many to process. Initially, I set up a data line
for each and processed the paths separately. That lasted until the first time I
tried it with less than the maximum and some blocks didn't execute because some
input pins were nul. What is the "elegant and simple" way to deal with this?
Drew Harrison
HP Microwave Test Accessories
707-577-3630
_______________________________________________________________________
I am currently testing a new e-mail client called Outlook.
If present, please disregard the "winmail.dat" attachment.
_______________________________________________________________________