AnsweredAssumed Answered

E2050A,VEE,SICL & EOI management

Question asked by VRFuser on Jan 21, 1999
Hi all,

First of all, maybe this message should be addressed to other forum but ...

We have detected what we consider a malfunction y the E2050A LAN/HPIB gateway.
We do need to assert the EOI line after a write transaction for commanding a
device which is connected to the E2050A.

We're using VEE 5.0 as control software. Trhough the menu 'Instrument
Manager --> Device Configuration --> Advance Device Configuration' we set
the option 'END (EOI) on EOL' to 'YES'.
But the E2050A did not assert the line and hence the handsahking is not
finished and I/O operation can not be executed.

It works properly if using a HPIB PCI card.

SICL version is G.

Any solution, advice or workaround?

Thanks in advance.


-------------------------------------------------
| Juan Vera                         |
| E-mail:     jvera@mdr.indra-espacio.es     |
| Phone:     34-913 963 986               |
| Fax:          34-913 963 912               |
| Earth Stations Department               |
| INDRA ESPACIO S.A.                    |
| Mar Egeo 4, Pol. Ind. 1               |
| San Fernando de Henares               |
| 28850 MADRID                         |
| SPAIN                              |
-------------------------------------------------


Outcomes