Hi,
I am running NT with HPVee 4.01. I want to start a DLL from within HP Vee,
then execute a DLL function that will go off asynchronously and perform some
task. While the task is being performed down in the DLL I want to go off and
do something else in HP Vee. When the task is done is it possible to notify
HP Vee through an event/message that the task is done?
I would like to do this instead of having to poll the task to see if it is
done.
I would appreciate help.
Mike Gustin
mgustin@smsmfg.sme.siemens.com