Dear Ralf,
usually every serial driver has his own problem. I think the problem is that
you clear the Buffer and you will have a timing problem. So here we need a
workaround which fits for you. Maybe it is possible to start one block
earlier to read the data's? Perhaps it is possible to start buffer clearing
before you get the trigger command? Did you try to read serial data's with
another program. Perhaps it can be a solution to read Data's in a Visual
Basic program.
That are only some ideas because I don't know the problem exactly.
Best regards
Barbara Aufenanger
------------------------------------------------------------
Somatec B. Aufenanger & M. Bernhardt
Jagdweg 7a
D-82041 Deisenhofen
Telefon : (089) 613 984 91
Fax. : (089) 613 981 23
Email : Aufenanger@somatec.de
homepage : http://www.somatec.com
------------------------------------------------------------
-----Original Message-----
From: ralf.eichele@smart-gmbh.de
[mailto:ralf.eichele@smart-gmbh.de]
Sent: Wednesday, February 10, 1999 9:07 AM
To: 'hpvxd_xc@hpislsup.lvld.hp.com'
Subject: Antwort: RE: sicl32.dll and and 8 serial ports
Hello Barbara,
First, we use WinNT. The Problem are not the single Threads. The
Devices we
connected send max. every 20 ms Data the a serial port. We've got a
buffer
of 2048K. The threads are seperated. The problem is that we clear
the
buffer, when Data is coming from the Devices. I think the problem is
not
VEE. The problem must be the buffer handling via SICL. Any
suggestions?
Greetings
Ralf
Hello Barbara,
First, we use WinNT. The Problem are not the single Threads. The Devices we
connected send max. every 20 ms Data the a serial port. We've got a buffer
of 2048K. The threads are seperated. The problem is that we clear the
buffer, when Data is coming from the Devices. I think the problem is not
VEE. The problem must be the buffer handling via SICL. Any suggestions?
Greetings
Ralf