SMART Electronic Development GmbH - Germany
Von: Ralf Eichele@SMART GMBH am 10.02.99 09:22
An: hpvxd_xc@hpislsup.lvld.hp.com
Kopie:
Thema: VRF: Error 979
Hello everybody,
since we use VEE 5.01, we get often the red screen with error number 979
and an error with signal 11.
Why get we sometimes this fault?
Greetings
Ralf Eichele
some times ago I got serious problems with my VEE programs. Many
irregular segmentation violations occurred (ERROR 979). But the
problems were only on my own PC ( VEE5.01). The same programs
worked fine with my colleagues PC (VEE5.0). So I thought it's a
hardware problem memory, gpib card or so. I began to swap hardware
components but without success. Found the problem. The programs are
running successful on every PC without installing the VEE5.01Patch. So
I think the segmentation violations are connected with the Patch. All
programms are calling the HPE1415E VXI PNP driver.
Is this a known problem ?
And I have another question.
We are using HP TestExecSL V2.1 with VEE actions. Since we use VEE5
with the corresponding VEEServiceManager it's impossible to debug
these actions unless all preceding actions are debugged. It disturbs
me especially in large testplans.
Is there a solution for this problem ?
Regards Christian
christian.wienhold@biotronik.de