AnsweredAssumed Answered

VRf-sequencer logging

Question asked by VRFuser on Jun 5, 1996

To whom concern or have answers to the following,

  I have been using and experimenting with this VEE software and
what I have found about the  logging output on the sequencer
object is not as immediate or ontime as expected , and this impair
the intention of using such output for monitoring purposes.
For monitoring results , I would like to see an almost immediate
results after execution of a particular test in the sequence is done.
What actually happen is logging output will only available at completion
of all tests in the sequencer.

  Normally for monitoring immediate results for tests in the sequencer,
tabulation format is necesary for readability, but logging do
only provide record out and to provide tabulation on screen will
need extra programming.

  Similarly for the spec in the sequencer, it would be nice if
the test spec can be summarised in a file/files, also spec can be inputed from
files(File driven). 


--

Best regards,
===========================================================================
BAHARI (MAT BAHARI )            Internet mail : bahari@comm.mot.com
Motorola Penang 604-6432511 (ext 4571) X400   Acount : CMB011
Malaysia.                                                           
===========================================================================



--

Best regards,
===========================================================================
BAHARI (MAT BAHARI )            Internet mail : bahari@comm.mot.com
Motorola Penang 604-6432511 (ext 4571) X400   Acount : CMB011
Malaysia.                                                           
===========================================================================

Outcomes