VRf-Need_help on Digital I/O speed.
to: VRf
from: Dave Lukert email: dave@viper.geg.mot.com
Motorola, Inc. GSTG Scottsdale, AZ
I have an application in which I need to generate two short,
simultaneous sequences of TTL signals at greater than a 2 kHz rate.
I have a HP E1458A 96-Ch Digital I/O VXI card which I am controlling
over the HP-IB through a HP 1406A Command Module.
Is it possible to generate bit patterns from the E1458A at this rate
using the HP-IB? Or do I need to use a GPIO card?
----------------------------------------------------------------------