Hello everybody,
I loaded the instrument driver file of HP8592B Spectrum Analyzer to the HP VEE
Evaluation software. Then it asked for the gpib.dll file. I also loaded that file.
But when I tried to "get the instrument",it gave an error message as follows:
"Error occured during load of device State Driver
Configuration error.Open gpib0 failed on National card
File "was not found
Make sure the National SBus card is installed properly with
the correct permission on the /dev file"
What can be the cause of that error?
Thanks.
Ozge Sahin
I loaded the instrument driver file of HP8592B Spectrum Analyzer to the HP VEE
Evaluation software. Then it asked for the gpib.dll file. I also loaded that file.
But when I tried to "get the instrument",it gave an error message as follows:
"Error occured during load of device State Driver
Configuration error.Open gpib0 failed on National card
File "was not found
Make sure the National SBus card is installed properly with
the correct permission on the /dev file"
What can be the cause of that error?
Thanks.
Ozge Sahin
gvg@lvld.hp.com / 970-679-3030 / FAX 970-679-5971
to: VRF-Ozge Sahin
date: Wednesday, 22 May 1996 0819 MDT
> I loaded the instrument driver file of HP8592B Spectrum Analyzer to the HP VEE
> Evaluation software. Then it asked for the gpib.dll file. I also loaded that file.
> But when I tried to "get the instrument",it gave an error message as follows:
>
> "Error occured during load of device State Driver
> Configuration error.Open gpib0 failed on National card
> File "was not found
> Make sure the National SBus card is installed properly with
> the correct permission on the /dev file"
"Sbus card"? That's for a SUN. Are you trying to use the VEE evaluation kit
on a Sun? It only works on a PC.
In any case, what National software and hardware do you have?
> What can be the cause of that error?
> Thanks.
> Ozge Sahin
[<>] regards -- gvg