AnsweredAssumed Answered

VRf - Error while compiling

Question asked by VRFuser on Mar 26, 1997
Item Subject: cc:Mail Text

Subject: VRf - Error while compiling
Author:  Conor Buescher at HP-Corvallis,om2
Date:    3/27/97 12:00 PM


     Hello,
    
     I've recently upgraded to Vee4.0 and have encountered a error while
     compiling Vee 3 code to Vee 4.0.
    
     The error message is:
    
                XIO:  fatal IO error 12 (Not enough space) on X server     
                "servername:0.0" after 23944 requests (23868 known         
                processed) with 62771 events remaining.
    
     I think I'm running out of memory during the creation of the p-code,
     but I'm not sure as to how to avoid it.
    
     This error occurred after hitting "save" on the default preferences
     menu. 
    
     The file that I'm converting to Vee4 is ~3.5Megs in size for Vee3
     compatibility mode.  (i.e., quite large)
    
     I'm on a HP 745i UNIX workstation with 64Megs of Ram.  I did not
     receive this error message under the Veebeta Roadrunner version.
    
     Any help??
    
     Thanks,
    
     Conor Buescher
    

.......................................................................

TO: hpvxd_xc@hpislsup.lvld.com
CC: Buescher_Conor/HP-Corvallis_om2@hp-pcd.cv.hp.com

Outcomes