Hi all:
Is there any way to have vertical fonts within VEE ?
Note.- It would be nice to have the posibility of rotating objects such as
labels in the panel view. In other words, a method of selecting the
orientation of these objects, i.e. [horizontal|vertical].
Juan Vera <jvera@mdr.inisel-espacio.es>
Indra Espacio S.A.
Is there any way to have vertical fonts within VEE ?
Note.- It would be nice to have the posibility of rotating objects such as
labels in the panel view. In other words, a method of selecting the
orientation of these objects, i.e. [horizontal|vertical].
Juan Vera <jvera@mdr.inisel-espacio.es>
Indra Espacio S.A.
gvg@lvld.hp.com / 970-679-3030 / FAX 970-679-5971
to: Juan Vera / VRf
date: Wednesday, 31 July 1996 0928 MDT
> Is there any way to have vertical fonts within VEE ?
You mean rotated 90 degrees? Not in normal operation ... if all you want
is fixed text, you could probably create a bitmap of the text in a paint
program, rotate it 90 degrees, and then use a Bitmap widget to load up the
bitmap ... but that's pretty klugey.
> Note.- It would be nice to have the posibility of rotating objects such as
> labels in the panel view. In other words, a method of selecting the
> orientation of these objects, i.e. [horizontal|vertical].
Some of them do (some indicators for instance). No previous requests for
rotating labels, however ...
> Juan Vera <jvera@mdr.inisel-espacio.es>
> Indra Espacio S.A.
If you have other questions, let us know.
[<>] regards -- gvg