AnsweredAssumed Answered

problem with Confirm button

Question asked by VRFuser on Apr 10, 1997
I am having a problem using Confirm buttons in panels.  They work find if I use "Show Panel On Execute", but
if I use the showPanel function the Confirm buttons are not activated the first time the function is executed.
If the program is stopped and the function is re-executed it will always work correctly from then on.

I am running VEE 3.21 on Windows NT 4.0 and HP-UX.  Both exhibit the same behavior.

Is this a known bug?  Any workarounds?  Is it fixed in VEE 4.0?

Thanks,
--------------------------------------------------------
Name: Tom Sanders
E-mail: toms@symca.com (Tom Sanders)
Date: 04/11/97
Time: 11:06:59
--------------------------------------------------------


Outcomes