> > Has anybody had trouble with Vee 4.1 randomly not finding drivers when
> > starting up? When I start VEE the message that a driver is not found,
> > would you like to install it now pops up. The driver listed is different
> > every time. The vee.io file lists the driver in question. This doen't
> > happen everytime I start VEE. VEE 3.2 doesn't do this. It only does it
> > on my Compac166. It works on a Compac133 on the shop floor. VEE Tech
> > Support never heard of the problem and suggested re-installing VEE,
> > which didn't help.
> > Andrew Kronquist
> > akronqui@burdick.com
I ran into a similar problem a little while ago. It turned out the default
directory in the Windows95 registry file had gotten changed. When I re-set it
back to where the drivers were actually at everything worked fine.
Allen K. Lair
alair@lois.dgim.doc.ca