AnsweredAssumed Answered

VRF-RE Main panel position in run time mode.

Question asked by pcconsultant on May 14, 1998
>Hello all:
>I have a problem with the Main panel position in run time mode.
>I create a program icon to run my program.vee.
>I want this program opens in the middle of screen but when I execute it
>shows each time in a diferent place.
>How can I fixed?
>Thanks,

Placement of the panel during development seems to affect the runtime
placement, but also look up "GEOMETRY" as a runtime command-line parameter.
It can help you to consistently place the main panel when the application
starts..
Allison Parker

>Isabel Gonzalez
>E-mail: gonzalez.i@ikusi.es
>Phone: 43-43-450800
>Fax:43-43-465220


Outcomes