AnsweredAssumed Answered

lap top and A/D boards

Question asked by VRFuser on Mar 11, 1999
Latest reply on Mar 11, 1999 by VRFuser


On Thu, 11 Mar 1999, Helena Frndova wrote:

> I'm using an PC with the Data Translation A/D board running application
> under HP VEE 4.01. Recently, there came a request to get more mobile and I
> was just wondering, if there is a possibility to run this from a lap top.
> Is anybody using PC A/D with a lap top? If yes, what requirements are here
> to meet?

Data Translation makes two PCMCIA boards that use the same excellent HPVEE
interface as their other boards.  We have been using the 7102 which has
both A/D and D/a with a Toshiba laptop with excellent results. These
boards are not supported under W98, only W95 and there are no plans
according to DT tech support to add W98 support for these cards.

Does anybody out there know of another manufacturer of a PCMCIA card with
a _hardware clocked_ D/A converter that interfaces elegantly with VEE?


Outcomes