AnsweredAssumed Answered

VRF Constructing Panels from Sub-Panels

Question asked by VRFuser on Jul 7, 1999
Using an HP34970A with...
1) 20 Chan MUX
2) Multifunction Module

I'm in need of help in the following area:

measuring both DC voltage and current when Chan 1 is closed. I can get the
voltage on chan 1 but when I try to go to Chan 21 for the current
measurement it Opens Chan 1 back up and no Cigar. Is there a way to open
multiple Channels when taking a single measurement?

Thanks


_______________________________________________________________
Get Free Email and Do More On The Web. Visit http://www.msn.com

Outcomes