Hi All,
I'm attempting to create a screen capture program to capture the screen
from a 8752C or 8753D. This appears to work fine, however the screen that
is captured has the 'COPY OUTPUT COMPLETED' display included !!!
Is there a way to suppress this message, or not allow it to be printed ?
Any help on this would be greatfully appreciated.
Thanks
James
(James.Atkin@Phase.Com)
I'm attempting to create a screen capture program to capture the screen
from a 8752C or 8753D. This appears to work fine, however the screen that
is captured has the 'COPY OUTPUT COMPLETED' display included !!!
Is there a way to suppress this message, or not allow it to be printed ?
Any help on this would be greatfully appreciated.
Thanks
James
(James.Atkin@Phase.Com)
> Hi All,
>
> I have wrote a little routine in VEE 4.01 that goes out on the RS-232
> bus every 40 minutes, over a period of several hours, and reads an
> instrument . Problem is that everytime I run the program I get an error
> message that says I/O time-out.
Do you ever get it to communicate? If not then your parameters
(baud rate, handshaking) may be wrong and mismatched to the remote
unit's.
Can you get the remote to communicate with a terminal program?
One useful trick is to find a laptop computer and see if you can
communicate between that and VEE as a debugging step.
[<>] regards -- gvg
>
>
> I'm sure that there is probably an easy fix that I'm not thinking of. I
> would greatly appreciate any advice I can get to help me fix this
> problem.
>
> Thanks,
>
> Dave Woodward
> Calibration Support Specialist
> BOEING Information & Support Systems
> M/S: 8H-44 Phone: (253)773-4256
> david.c.woodward@boeing.com