I have a test station that I have inherited from another designer.
My task is to develop a second test station using the Vee programs
from station #1. My problem:
Station 1 is UNIX 9.0 running Vee 3.2
Station 2 is UNIX 10.2 running Vee 4.0
When I import the Vee files to station 2 and run Vee in 3.0
compatibility mode, it takes at least twice as long to complete
each routine. REALLY SLOW!! Should I expect this, or should I
expect that Vee 4.0 running in 3.0 compatibility mode would process
through at the same rate as if it was running on a 3.2 station?
Please help.
Michelle Farris
650-813-2279
michelle.farris@stellexms.com
Test Engineer
Stellex Microwave Systems
3333 Hillview Ave
Palo Alto, CA 94304