AnsweredAssumed Answered

Vee 4.0 run in 3.0 compatibility mode

Question asked by VRFuser on May 27, 1998
Michelle Farris wrote:

>      I have a test station that I have inherited from another designer.
>      My task is to develop a second test station using the Vee programs
>      from station #1.  My problem:
>
>      Station 1 is UNIX 9.0 running Vee 3.2
>      Station 2 is UNIX 10.2 running Vee 4.0
>
>      When I import the Vee files to station 2 and run Vee in 3.0
>      compatibility mode, it takes at least twice as long to complete
>      each routine.  REALLY SLOW!!  Should I expect this, or should I
>      expect that Vee 4.0 running in 3.0 compatibility mode would process
>      through at the same rate as if it was running on a 3.2 station?

No, it should run the same speed (ALL OTHER THINGS BEING
EQUAL!)  This is a new one on us.

[%%] regards -- gvg

>
>
>      Please help.
>
>      Michelle Farris
>      650-813-2279
>      michelle.farris@stellexms.com
>
>      Test Engineer
>      Stellex Microwave Systems
>      3333 Hillview Ave
>      Palo Alto, CA  94304




Outcomes