AnsweredAssumed Answered

vrf Dr Who was Marker color values and position info

Question asked by hansolofalcon on Dec 7, 2001
Hello from Gregg C Levine
You are? Okay now the important question. Which one? Number One, or
Number Two? Or even the ones after that? I am a fan of Numbers Four, and
Seven, and to a lesser extant Number Eight. And is there room for me? I
am a fan of his from way back after all.
-------------------
Gregg C Levine hansolofalcon@worldnet.att.net
------------------------------------------------------------
"The Force will be with you...Always." Obi-Wan Kenobi
"Use the Force, Luke." Obi-Wan Kenobi
(This company dedicates this E-Mail to General Obi-Wan Kenobi )
(This company dedicates this E-Mail to Master Yoda )



> -----Original Message-----
> From: owner-vrf@lvld.agilent.com [mailto:owner-vrf@lvld.agilent.com]
On Behalf
> Of Shawn Fessenden
> Sent: Saturday, December 08, 2001 11:34 AM
> To: vrf@lvld.agilent.com
> Cc: valhalla@quixnet.net
> Subject: vrf: Marker color values and position info
>
> Hi Hal.
>
> >Is it possible to have different
> >color values for each marker when
> >you have two markers on a display
> >object?
>
> Hal, I'm sorry to say, "not in this lifetime". Different colors on
markers,
> dynamic marker readout and no mouse halt are things the XY Trace
simply
> won't do.
>
> However (you knew this was coming, didn't you?
>
> Because of an extraordinary act of kindness on the part of one Scott
H. in
> the alt.binaries.drwho newsgroup I'm using this weekend to replace the
XY
> Trace object. In fact, I'm so **** happy that the Scope ActiveX
control *and
> it's source code* are unlicenced public domain entities. Yes, I too
have
> fought that stupid licence stuff in VEE.
>
> I'm not going to sit here and claim that this control is every bit as
> functional as Agilent's or better, but it can be made so by others if
they
> wish. As supplied, this control will simply do what you want, without
all
> the right-click niceties of Agilent's version.
>
> So sit back and relax. Monday morning your control will be in your
inbox and
> Sunday night at 11:00 pm. I'll be taking a trip back in time with Dr.
Who.
> -SHAWN-
>
> _________________________________________________________________
> Get your FREE download of MSN Explorer at
http://explorer.msn.com/intl.asp
>
> ---------------------------------------------------------------------
> This is the "vrf" maillist, managed by Majordomo.  To send messages to
> this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions
and
> unsubscriptions are done through the address
"vrf-request@lvld.agilent.com".
> If you need details, just send a message containing the text "help"
> to "vrf-request@lvld.agilent.com".
> ---------------------------------------------------------------------

---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes