On Fri, 15 Jan 1999, Bernhard Muller wrote:
OOPS! These commands are specific to Data Translation cards. Sorry if
the question is inappropriate.
>
> I need to be able to configure a D/A converter to output from a file
> continuously. This is easy with a single Config D/A object properly
> configured and a startacq object.
>
> Next, I need to be able to turn the signal off and on from the panel in a
> running program. This is also easy.
>
> What I cannot seem to be able to do is turn off the running acquisition
> and restart it with a different filename. I have tried using get/set
> datamode objects, and have tried using different D/A config objects. Can
> this be done?
>
>
I need to be able to configure a D/A converter to output from a file
continuously. This is easy with a single Config D/A object properly
configured and a startacq object.
Next, I need to be able to turn the signal off and on from the panel in a
running program. This is also easy.
What I cannot seem to be able to do is turn off the running acquisition
and restart it with a different filename. I have tried using get/set
datamode objects, and have tried using different D/A config objects. Can
this be done?