Charlie,
Just use the I/O -> Execute Program(PC) object in vee. Add the control input
'command' and send it any dos command. Use the To String object or a formula
object to build a text string such as :
mkdir c:
ewdir
and send this to the above object. This should solve your problem.
Mike Asbery
At 10:21 AM 7/14/99 -0400, Spellman, Charlie wrote:
>
> Hello everyone
>
> Is it possible(and how) to create a new folder in a directory from a
> VEE(5.01, Win 95 or NT) program. The user will input via a text box a part
> number, and I would like to then create a folder based on that part no (if it
> already does not exist) to store the data. I tried to just put the path name
> (with the new folder name) into the filename input of a To File object, but
> that gave me an error (700, file not found).
>
> Thanks
>
> Charlie Spellman
> RF Systems Engineer
> RFS Cablewave Systems
> 200 Pondview Drive
> Meriden, CT 06450
> (203) 630-3311
> <mailto:spellman@cablewave.com>spellman@cablewave.com
***********************************************************
Michael N. Asbery, NRL Code 5733.20, (202)404-3014, DSN 357
michael.asbery@nrl.navy.mil fax (202)404-7661
***********************************************************
Just use the I/O -> Execute Program(PC) object in vee. Add the control input
'command' and send it any dos command. Use the To String object or a formula
object to build a text string such as :
mkdir c:
ewdir
and send this to the above object. This should solve your problem.
Mike Asbery
At 10:21 AM 7/14/99 -0400, Spellman, Charlie wrote:
>
> Hello everyone
>
> Is it possible(and how) to create a new folder in a directory from a
> VEE(5.01, Win 95 or NT) program. The user will input via a text box a part
> number, and I would like to then create a folder based on that part no (if it
> already does not exist) to store the data. I tried to just put the path name
> (with the new folder name) into the filename input of a To File object, but
> that gave me an error (700, file not found).
>
> Thanks
>
> Charlie Spellman
> RF Systems Engineer
> RFS Cablewave Systems
> 200 Pondview Drive
> Meriden, CT 06450
> (203) 630-3311
> <mailto:spellman@cablewave.com>spellman@cablewave.com
***********************************************************
Michael N. Asbery, NRL Code 5733.20, (202)404-3014, DSN 357
michael.asbery@nrl.navy.mil fax (202)404-7661
***********************************************************
We have bought a scope card from Gage Company (CS8012APCI) but we have
found out that they do not produce the drivers for the HpVee. In order to
use card from Hpvee first I have written a dll in VC++6.00 and used in my
HPVee program. But I have some problems.
I wonder if someone has worked on Gage devices with HPVee.
-----------------------------------------------------------------------
Cagri Acar
Test Engineer
ASELSAN A.S.
email:cacar@mst.aselsan.com.tr
Http :http://www.eee.metu.edu.tr/~e102231