AnsweredAssumed Answered

Manufacturer supplied DLL and HP VEE

Question asked by VRFuser on Jul 14, 1999
Hi, All

We would like to control one external device connected to the parallel
port using VEE4.0.
There are a .DLL, .LIB and .H files about which is said that they can be
easy
used with any VisualBasic, Pascal or C-Program.

Unfortunately, as we found from the driver manual and .H file,
there are several  parameters of specific types :
HWND, HANDLE, WORD.
As far as we understand these are specific Windows variables.

As followed from the manual of HP VEE, it does not
support  such types.

How we can solve the problem?

Regards. George.
--
George Onishchukov

Institute of Applied Physics
Friedrich-Schiller-University of Jena
Max-Wien-Platz 1
D-07743 Jena
Germany

Phone:   +49 3641 65 76 60
Fax:     +49 3641 65 76 80
e-mail: George.Onishchukov@uni-jena.de



Outcomes