AnsweredAssumed Answered

Troubles with Main Panel position using Run time mode

Question asked by VRFuser on May 14, 1998
Isabel Gonzlez wrote:

> Hello all:
> I have a problem with the Main panel position in run time mode.
> I create a program icon to run my program.vee.
> I want this program opens in the middle of screen but when I execute it
> shows each time in a diferent place.
> How can I fixed?



Madam:

Try these steps:

% Make sure you have updated to VEE 4.01
   (you can use www.hp.com/go/vee to get the patch).

% Make sure you have a main panel in your program
   when you build it and that you run it, get the
   execution window, and then place the panel properly.

% You can then secure the program as a runtime
  program.

You should have no further problems.

[<>] regards -- gvg

> Thanks,
>
> Isabel Gonzalez
> E-mail: gonzalez.i@ikusi.es
> Phone: 43-43-450800
> Fax:43-43-465220




Outcomes