cebollerocj@inta.es wrote:
>
> Hello everybody;
Hallo!
> ...
> We have added the hardware in
> adding hardware, but when we try configure the card with the
> I/o_config we cant do it and says that there is no HP82335 card in
> the computer.
May be there is a conflict with your IRQ or IO settings?
Can you assign the network card to another interrupt and
try again?
I also remember that I read something on HPs web page
concerning the config of these cards (as system controller).
But if the card works in the other computer it shouldn't be
the problem...
With kind regards.
Heiko.
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo. To send messages to
this maillist, just email to "vrf@lvld.hp.com". Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.hp.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.hp.com".
---------------------------------------------------------------------