----- Oorspronkelijk bericht -----
Van: Robert Rais <rrais@yazaki-na.com>
Aan: <hpvxd_xc@hpislsup.lvld.hp.com>
Verzonden: dinsdag 24 augustus 1999 8:30
Onderwerp: VRF: LAN HPIB Gateway
Has anyone configured a LAN HPIB gateway before. I am evaluating one and
having minor difficulties. Any help would be appreciated.
Robert Rais
Engineer
Yazaki North America Inc.
Testing and Reliability
rrais@yazaki-na.com
Direct:734-983-6444
Fax: 734-983-6445
Yes, Robert
We have HP E2050A HP/IB - LAN gateways with different data acquisition
systems ( HP 34970A and HP 3852A ) on one HP Vectra PC with Windows NT4.
We worked with gateways on two ways:
- a network from BNC coax cable ( RG58) and 50 ohm resistence (R404 441) at
both ends of the cable.
- a network from twisted pair cable .
You have to give the gateways different IP addresses. This you can do with
TELNET
In the HOSTS file ( c:winntsystem32driversetchosts ) you have to map
the IP addresses.
For the application HPVEE, you have to configured in HP_IO_libraries
IO_config) a LAN Client.
In HPVEE (version 5.01) you have to change in the instrument manager
I/O) ( edit instrument, device configuration ) the gateway item from "this
host" in the new IP address.
regards
Odoorn,
Jan Klingenberg
The Netherlands
klingenberg@wxs. (home)
j.klingenberg@gasunie.nl (work)
Robert Rais
Engineer
Yazaki North America Inc.
Testing and Reliability
rrais@yazaki-na.com
Direct:734-983-6444
Fax: 734-983-6445