AnsweredAssumed Answered

vrf Network Runtime

Question asked by VRFuser on Feb 20, 2000
I loaded a run time version to a network server.  I e-mailed short cuts to
all of the users that pointed to the networked drive.  My application would
only be used by one user at a time since all users shared a common file.

Tom Mitchell
Visteon Automotive Systems
Software Validation/Product Assurance
ETC Room B116
17000 Rotunda Drive
Dearborn, MI 48121
Voice/FAX number: (313) 323-9518    Text pager:(313) 795-2709
EMAIL:tmitchel@visteon.com        
textpager 3137952709@alphapage.airtouch.com



-----Original Message-----
From: Anderson, Scott [mailto:Scott_Anderson@adc.com]
Sent: Monday, February 21, 2000 9:03 AM
To: 'vrf@lvld.hp.com'
Subject: vrf Network Runtime


Hello all

Has anyone installed the Vee runtime to a network drive and used that to run
their executables?
Is it even allowed by HP?
I have about 30 computers to maintain in production and was hoping to find a
way, not to have to load the runtime
on each one of them.  They are all running now but in the future it would be
nice not to have to do it.

thanks for your help,

Scott Anderson
Process Development
ADC Telecommunications
BCG Wireless
1100 N 4th St.
LeSueur, MN 56058
1-800-366-3889 EXT.4784
scott_anderson@adc.com

---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.hp.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.hp.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.hp.com".
---------------------------------------------------------------------
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.hp.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.hp.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.hp.com".
---------------------------------------------------------------------

Outcomes